Industry Online Support
Technical Forum
2/11/2008 9:19 PM | |
Posts: 177 Rating:
|
Hi, In the zip file I have attached the script used as well as the results that were written to the user archive and what was displayed in the runtime window in WinCC from the printf statements. Basically, the aim of the script is to transfer the contants of a user archive from one WinCC system, to another. These systems are independant and we have used an OPC connection to write the original values to tags on the other system. The script was running fine for about two weeks, then just went crazy for no apparent reason. There apears to be nothing out of the ordinary that triggered this. Do the commands for the connecting, opening, writing and closing of the user archives look OK? Is there anything else that I should be looking for, or is there a better way to solve this problem. Thanks in advance, henno2000 AttachmentUA.zip (49 Downloads) |
2/14/2008 5:15 PM | |
Joined: 2/14/2008 Last visit: 9/22/2023 Posts: 2 Rating:
|
Are you using a Redundant Server with UA? |
Keith M Welch |
|
Follow us on