11/23/2005 4:14 PM | |
Posts: 8 Rating: (1) |
After installation of the WinCC v.6 SP3 in Windows XP SP2, alarm logging does not function, does not allow to keep alterations.[:cry:] |
1/16/2006 8:23 AM | |
Posts: 3149 Rating: (171)
|
Hi Peri, where are the alarms generated: in your S7 via SFC/Alarmblock or via internal variables in WinCC? Regards, Nemo |
1/16/2006 1:04 PM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (151)
|
There appear to be two different questions in this thread ! Regarding them both, I believe that Hotfix 3 fixes some issues with the Alarm Logging in V6SP3. I would recommend you both contact the hotline and if necessary they can send you hotfix 3. To log a case with the hotilne, go to http://support.automation.siemens.com/WW/view/en/16605654 Regards, Salma |
Follow us on