2/12/2021 4:44 PM | |
Joined: 9/1/2017 Last visit: 5/19/2024 Posts: 156 Rating: (19) |
Hi
In wincc explorer--> tag logging-->archive configuration-->Rclk on tag logging fast and slow--> reset Alarm logging-->archive configuration-->Rclk on message archive--> reset Regards AttachmentMicrosoft-Windows-Server_en_2021-02-11.xlsx (180 Downloads) |
2/19/2021 9:44 PM | |
Joined: 9/1/2017 Last visit: 5/19/2024 Posts: 156 Rating: (19) |
Hi Had your project worked fine before? Is it integrated pc station or stand alone wincc project? Regards Edit: Please take a look at Why does enabling of the Runtime (WinCC V7 and WinCC Professional) freeze with "Alarm Logging Runtime" or "Tag Logging Runtime"? |
Last edited by: hosein8419 at: 02/20/2021 12:13:15Last edited by: Jen_Moderator at: 02/22/2021 09:02:47Optimized link. |
|
This contribution was helpful to1 thankful Users |
2/22/2021 8:37 PM | |
Posts: 13 Rating: (0) |
schufri and hosein8419, So I followed what hosein8419 linked earlier; Please take a look atWhy does enabling of the Runtime (WinCC V7 and WinCC Professional) freeze with "Alarm Logging Runtime" or "Tag Logging Runtime"? Note: I did all 4 possible remedies none worked. It recreated the ALG and TLG files in both .ldf and .mdf Interesting that Siemens puts Message Queuing to start automatically. When you install WinCC v7.5 it does that automatically and will throw alarms on the server if it isn't running. The project works in WinCC V7.3 and is currently running on another server. I will use the project duplicator and convert again and let you know. More later. |
Last edited by: ChrisH_ATL at: 02/26/2021 15:40:39 |
|
This contribution was helpful to1 thankful Users |
2/26/2021 4:32 PM | |
Joined: 9/1/2017 Last visit: 5/19/2024 Posts: 156 Rating: (19) |
Hi You are using step7 tia portal v14 for s7-1200? I guess the problem may refer to the compability of your winncc and tia portal version. As i checked in Siemens compatibility tool you must have tia portal v16 to be compatible with wincc v7.5 sp1. Can you check this? Hope this helps Regards |
Follow us on