1/30/2012 3:09 PM | |
Joined: 9/28/2005 Last visit: 5/23/2024 Posts: 2957 Rating: (242)
|
Hi, Well officially Flexible 2007 is supported on Windows XP Pro SP1, but you could check following link and try out new compatibility tool to see if you have compatibility issues or not. http://support.automation.siemens.com/WW/view/en/22055368 By the way, from which media you are trying to install Flexible ? DVD or via network ? |
Best regards, |
|
1/31/2012 6:10 PM | |
Joined: 11/9/2008 Last visit: 6/3/2024 Posts: 404 Rating: (6) |
HI Darius, I have copied setup from DVD to my local drive still the same problem persist. Regards, Yogendra G.
|
5/1/2012 1:27 PM | |
Posts: 272 Rating: (4) |
stop wincc sql server andthen try to install flexible...it might work,,, |
5/2/2012 8:26 AM | |
Posts: 8946 Rating: (999) |
WinCCflex 2007 will run fine also under XPpro SP3. |