5/2/2009 1:01 PM | |
Joined: 11/9/2008 Last visit: 1/20/2023 Posts: 398 Rating:
|
Dear All, I have copied 2 screen from diffrent project in my project after copy the screen.When i compile the project one window is appere "Select HMI Device to Generate" in this window two devices is showing Device_1 and Device_2. In my Project decive name is 1 then i don't understand who it is come? If i want to remove this device how i can remove? Plz suggest me. I'm sending u one snap shot for ur refrance. Regards, Yogendra G AttachmentDevice.zip (56 Downloads) |
This contribution was helpful to
1 thankful Users |
5/5/2009 10:42 AM | |
Joined: 11/9/2008 Last visit: 1/20/2023 Posts: 398 Rating:
|
Dear Manfred, I'm not able to do that can u send me Snap Shot for this Procedure. Regrads, Yogendra G |
Follow us on