1/4/2016 8:22 PM | |
Posts: 68 Rating: (0) |
Hey guys, I'm running the following : * Windows 7 professional 32bit SP1. *WinccFlex 2008 SP3. *TIA Portal V13 SP 1 Update 4. *Step 7 V5.5 SP4. ______________________________________________________________________________________ So as mentioned in the topic, I am trying to migrate HMI project from flex to TIA but with no success As you can see in the attached log file it says that I have to be installed with WinCC flexible SP2 or SP3, although I have SP 3 installed. What am I doing wrong??!!! Regards, Woop_Ass AttachmentMigration log.txt (269 Downloads) |
1/4/2016 8:23 PM | |
Posts: 68 Rating: (0) |
FYI, I attached the software installed info from the TIA |
1/5/2016 8:42 AM | |
Posts: 68 Rating: (0) |
Thanks guys I'll give it a go... |
Follow us on