2/10/2012 8:04 AM | |
Posts: 10 Rating:
|
hi, i found the same cable works Windows XP ... but not with the Windows 7.. just now i checked.. Kindly advice me...
|
2/11/2012 6:58 PM | |
Posts: 10 Rating:
|
Please check this issue and give me a solution... |
2/13/2012 10:11 AM | |
Posts: 2348 Rating:
|
To be honest i don't understand why it's not working on ISO I see only 1 more thing to do - select TCP/IP -> Realtek PCIe GBE Famil... and TCP/IP(Auto) -> Realtek PCIe GBE Famil... via Setting PC/PG interface and try to reach your CPU via IP address (try both in XP and S7). If it pings it should be available - you can upload CPU configuration then to see CP settings (please specify correct slot number on uploading). |
2/13/2012 12:20 PM | |
Posts: 1547 Rating:
|
Hello Vijay.py01, Could you please postthe Ordernumber and Firmwareversion of your CP? There is a strong possibility that your Firmwareversion is to old to support newer versions of the DLC Protocol (DLC is used to detect your components over LAN). Also I found out, that your installed Step7 Version is only compatible with 32bit Windows 7 Installations - so please check that as well. You can checkthecompatibilityusing this tool: Compatibility Tool |
2/13/2012 1:18 PM | |
Posts: 10 Rating:
|
hi, Order number 6GK7- 443-1GX20-0XE0 Frim ware version V2.0 By default and i updated the frim ware version to V2.1.current version is V2.1. My PC is Windows ultimate 32 bit version i checked the compatibility it shows "compitable" |
2/13/2012 4:06 PM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hello Vijay, I know What I am going to say is you are already Tryed out But Still have a look on Point, 1. Connect Both your Windows XP & 7 Computer On the Same Network. 2. Try to assined the Same Series of IP. 3. Select TCP/IP (Auto) in Set PG/PC Interface. 4. then checked from one by one PC for the MAC address is detecting. also Checked when you connected the Cable to the Windows 7 PC are you able to ping the other PC IP on the network? |
Last edited by: Ammy at: 2/13/2012 4:07 PMAmmy |
|
Follow us on