10/22/2024 2:18 PM | |
Joined: 7/19/2022 Last visit: 1/17/2025 Posts: 433 Rating: (71) |
Hello Brad27243, Please note the measurement range limits for wire break detection, they must be 1...5 V or 4...20 mA. With the rest the function is not available: Parameter description analog input By default TIA Portal configures the 2-wire as 4...20 mA but the 4-wire as -20...+20 mA |
Last edited by: JBS98 at: 10/22/2024 14:19:11If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on