5/27/2011 1:27 PM | |
Posts: 272 Rating:
|
Hi All, Is it possible to have a wireless communication for a distance of 4 kms. |
5/27/2011 1:38 PM | |
Joined: 3/21/2006 Last visit: 3/19/2025 Posts: 10239 Rating:
|
Hello, Take a look at
If you keep to use Siemens look at Simatic S7-300 wireless?(almost the same issue but the required distance is less then yours. Other way is to use GPRS for the remote stations. And an Internet connection at the central location. In case of S7-300 SINAUT ST7 system http://support.automation.siemens.com/WW/view/en/23810112 In case of S7-200 SINAUT Micro solution: http://support.automation.siemens.com/WW/view/en/22537809 Best regards, Hristo Mihalev |
5/27/2011 1:38 PM | |
Joined: 10/7/2005 Last visit: 3/20/2025 Posts: 3042 Rating:
|
Yes it is Prats, Voyager 1 is at time of writing some 17,408,281,206 km away from Earth (see HERE for more) and still wirelessly communicating so you can surely communciate wirelessly over 4 km, wouldn't you agree? If you give us some details about the applicationand what sort of speed you need, we may even be able to give you advise on equipment that does not require usage of a rather large Satellite dish. |
Last edited by: fritz at: 5/27/2011 1:41 PMfixed typos Cheers |
|
5/27/2011 4:50 PM | |
Posts: 947 Rating:
|
Hi |
5/27/2011 4:56 PM | |
Posts: 8946 Rating:
|
Nice comparison. And here is the antenna equipment that you need! http://www.vla.nrao.edu/ |
Follow us on