Industry Online Support
Technical Forum
10/11/2009 1:58 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (309) |
Hello, A possible solution is to use GPRS for the remote stations. And an Internet connection at the central location. Have a look to the SINAUT ST7 system in this example: http://support.automation.siemens.com/WW/view/en/23810112 and more specially the volume 2 using GPRS For smaller CPUs (S7-200) there is also a SINAUT Micro solution: Here an example. http://support.automation.siemens.com/WW/view/en/22537809 |
Best regards |
|
This contribution was helpful to1 thankful Users |
Follow us on