10/31/2011 12:38 PM | |
Posts: 8 Rating:
|
Hello Amit, The problem is not so simple as it seems to be... Why?: If you try to use Webnavigator you have to redesignall the HMIscreens with associated Tags. A better solution is to keep the actual screens on WinCC and to use Simatic Net OPC Server to relink all the Tags from your applications from the Network. As a rule, if you use directional antennas,a distance of 30m it's not a problem. For BOM go to https://www.automation.siemens.com/mcms/industrial-communication/en/support/catalog/Pages/catalog.aspx?HTTPS=REDIR, download the catalogue and try to find what INS indicated but there are a lot of accesories...(Cables, C-Plug, Antennas...) which you have to choose for.. You also have to keep in mind that if you try to use the HMI screens for issuing commands in yourreal applications on the network, the time become critical. Good luck.... |
Follow us on