5/25/2013 12:20 PM | |
Posts: 90 Rating:
|
Hey guys! I want to install a 3-way signal isolator between an analog input module (6ES7331-7KF02-0AB0) and a 2-wire transmitter. I know the proper wiring of an AI module and transmitter based on the S7 manuals but I’m not sure about the wiring in the case of adding a signal isolator. However I have considered two different wiring diagrams as shown in attached file. Could you take a look at them and give me some advice on how to do to the wiring? Should I implement Figure-1 or Figure-2? |
5/25/2013 4:12 PM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, Fig 1 you use if the isolator is not powering the sensor by the 4 to 20 mA loop. Fig 2 you use if the isolator can power your loop. So wht's in the isolator specs? Regards, Marcjan |
Problem solved? |
|
5/25/2013 7:03 PM | |
Posts: 90 Rating:
|
Thank you Marcjan! The isolator catalog is attached. As you can see it needs a 24 VDC power itself and since the input and output are separated I don’t think it can provide the loop. What do you think? Attachmente_cat_083.pdf (331 Downloads) |
5/27/2013 7:16 AM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, You are right, so you can use Fig 1 to connect your sensor. Regards, Marcjan |
Problem solved? |
|
This contribution was helpful to
1 thankful Users |
6/28/2013 9:06 AM | |
Joined: 11/18/2010 Last visit: 8/5/2022 Posts: 523 Rating:
|
hi i think Fig 2 is right because in isolatoris providing power to ai ,so not need to provide external supply between plc and isolator. viral |
We are working on a new user interface with better overview and more relevance.
Follow us on