10/1/2021 8:19 AM | |
Joined: 4/20/2021 Last visit: 1/26/2023 Posts: 70 Rating: (0) |
Hi all, I'm interesting to write a python code in my iot siemens 2050 and I would like create a code which run as in PLC Siemens or better which loop continuously ( I don't remember the correct definition of this type of work). Have someone some information to create a python code which loop which check input pin, output pin and other paramenters. Maybe a library exists to avoid while or for loops? many thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/01/2021 09:18:04New subject after splitting |
|
10/1/2021 2:47 PM | |
Joined: 4/28/2015 Last visit: 9/9/2024 Posts: 3345 Rating: (379)
|
Hi, to have access to the in- and outputs of the IOT2050 we are using the mraa library. This is available on the IOT2050 and you find an example here. Originally for the 2040, but works for the 2050 as well. The example uses the I/O shield, if you don't use it, you can use the GPIO numbers as they are on the board. If you want to control the USER LED, you can find an example here. I don't know if there is anything out there for a more sophisticated loop, but I am sure you will find some results how to do that on google. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on