11/24/2023 12:29 PM | |
Joined: 9/28/2023 Last visit: 1/6/2025 Posts: 18 Rating: (0) |
Good morning, OK it works. Thanks but I have another question. Now I also have to write the same data to the client's network. 1° the customer’s network address is \\fsrv\Be\TEST BENCHES\04 - HOLD OPEN RODS BENCH - M01000\02 – REPORTS I guess I need to change the \ by / otherwise I'm helping errors in my script. 2° the client requests Name and password authentication. My question is where to put the Name and password provided by the customer?? Thanks in advance and have a good day. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/27/2023 08:09:19New subject after splitting |
|
11/24/2023 1:00 PM | |
Joined: 1/21/2013 Last visit: 1/24/2025 Posts: 3460 Rating: (543)
|
Hi Constantin/siemens, You cannot access a network source directly from your script. You can add this network source as a network drive, which you can access from within your script using '/net/mount'. Kind regards |
This contribution was helpful to1 thankful Users |
Follow us on