9/22/2020 9:24 AM | |
Joined: 2/12/2018 Last visit: 9/26/2023 Posts: 22 Rating: (0) |
Hello ! with regards to ( the Symbolic IO field) : A. Writing the list into the faceplate: I have implemented text lists inside faceplates. (in TIA 15) Can we do that in the unified environment? Without having to refer to a list from outside , it is more convenient if we have to use our already created faceplates in new projects. We don't have to copy them between projects. any tip please? B. Hide the drop-down arrow: I tried to set the property (Misc => Mode: Output) but the arrow still appears! (The behavior in the old touch panels is different! The arrow is hidden when this property is used.) any suggestion, please? thank you ... ------------------------------------------------------------------------------------------ |
Last edited by: Optimistic at: 09/22/2020 09:26:00Last edited by: Optimistic at: 09/22/2020 09:26:46Last edited by: Jen_Moderator at: 09/30/2020 12:43:17New subject after splitting |
|
10/17/2022 5:25 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (174) |
New question published by baioretto is split to a separate thread with the subject Include text lists in the faceplate to show some internal state of a component. Best regards |
Follow us on