7/13/2013 6:36 PM | |
Posts: 378 Rating: (73) |
Any Help? At least if there is a way to convert Tag names and alarm texts? Thanks |
7/13/2013 9:01 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
What kind of files are they? From that point of view perhaps it is possible. |
7/14/2013 10:56 PM | |
Posts: 378 Rating: (73) |
Hello UMENCHO, The file types are:
Note that I have tried to open this files with Notepad, Excel and I can not see meaningfull characters. Thank you! |
7/15/2013 12:38 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
So, there are 2 steps: 1. Export the tag dictionary from Zenon HMI in .csv format. Open the project -> Variable -> In local menu before filter icon has another one "Import S7 project". Click there and select "Export CSZ all". Save As -> select name and type of file. 2.How can you import/export configuration data (discrete and analog alarm messages, tags and connections) from/to a CSV file in WinCC flexible 2008? (create a project and one tag) export procedure 3. Open both files and copy/paste procedure...When the WinCC Flex file is prepared with all tags from Zenon HMI project, save and import it in WinCC Flex project. To be honest I found one document showing transfering the tags between Siemens 505 Workshop and Zenon HMI. Best regards, Hristo Mihalev
|
This contribution was helpful to1 thankful Users |
7/15/2013 3:22 PM | |
Posts: 378 Rating: (73) |
Hello UMENCHO, Many thanks for your great help. As you have said, I have exported to .csv format and I get tag name column and PLC adress column but the problem I have faced is PLC adress for example for adress DB8.DBW0 i get EDW (2) 008. 0000 . 000 But now I have made some excel formula to convert ZenOn adress format to SIMATIC format, and added to .csv tag lists. Now I am (you are) sucessfully converted the 950 Tags to wincc! I have concluded that I have no option to convert the graphic items, I should do it manually but it will take me two or three weeks.
Whould you like to give me this document? Thanks again and I owe you one! |
7/16/2013 7:11 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
As requested:http://www.copadata.com/fileadmin/user_upload/Downloads/Dokumentation/651SP0/ENGLISH/Manual/Import%20-%20Export.pdf?PHPSESSID=ea913840c23ec0053256c97c42330147 |
This contribution was helpful to2 thankful Users |