10/8/2021 6:23 PM | |
Posts: 257 Rating:
|
Hello SIOS-Forum-Community,
To upgrade a license key or an "old authorization" the following prerequisites are necessary prerequisites are required:
and the licence key or an "old authorisation" on an authorisation diskette.
- If the upgrade target is a licence key on the following storage locations: licence key data carrier or authorisation disk, drive or USB memory stick. - If the upgrade target is an authorisation: only on the authorisation disk. Performing a Licence Upgrade To upgrade a licence key (hereinafter referred to as a licence key, even if the source or target is an authorisation) source or target is an authorisation), proceed as follows. 1: 1. select the menu command "View > Manage". Select the location in the navigation area where the licence key is located, for which the upgrade is to be carried out. 3. In the object area, select the licence key for which the upgrade is to be carried out. is to be performed. 4. 4. execute the menu command "License Key > Upgrade". - If there is only one option for the upgrade, the upgrade is carried out without further displays and queries. - If several upgrade options are found, the "License Key Upgrade" dialogue opens. Upgrade" dialogue opens. - Select the upgrade to be carried out and click on the button "Upgrade". When upgrading licences, it is important to select the licence that is to be upgraded. Only then will the process work. If only the upgrade is selected, it will not work.
or in the online help of the current Automation License Manager. Note The procedure described in this article refers to the time of writing this article (status: April 2021). With kind regards
|
This contribution was helpful to
1 thankful Users |
Follow us on