4/22/2022 12:20 PM | |
Joined: 10/30/2018 Last visit: 9/19/2024 Posts: 8 Rating: (0) |
Hello Experts, How can i configure IEPBHA on 400 plc CP card ? |
4/22/2022 3:32 PM | |
Joined: 9/27/2006 Last visit: 10/17/2024 Posts: 12289 Rating: (2687)
|
Hello Avinash; Very sorry, are you refering to a IE/PB link HA, part number 6GK1411-5BB00? You need to tell us more about what you are planning to use this gateway for, as a simple gateway or as a Profinet IO device as well, see the screenshot below, This image is taken from the IE/PB Link manual: https://support.industry.siemens.com/cs/ww/en/view/109744280 The manual provides a huge amount of information on the IE/PB Link HA, such as the fact that it can be used for S2 redundancy with Profibus-DP slaves, and more. Starting on page 59 you eill find instructions for configuring the link with S7-400 CPUs, using Step 7 v5.6. If you still need clarifications, simply come back to the forum with more details on your project. Hope this helps, |
Last edited by: dchartier at: 04/23/2022 03:26:15 |
|
Follow us on