7/6/2022 11:31 AM | |
Joined: 7/15/2021 Last visit: 5/15/2024 Posts: 1 Rating: (0) |
Hello, Why it is not possible to programming with S7-Graph a IEC 60848 Grafcet like the attachement example. Regards. ------------------------------------------------------------------------------------------ AttachmentGraph.pdf (622 Downloads) |
Last edited by: The Helping Hand at: 07/06/2022 13:00:27New subject after splitting |
|
7/6/2022 4:23 PM | |
Joined: 7/7/2010 Last visit: 11/15/2024 Posts: 15402 Rating: (2443) |
As to why it is not possible to do something, as with all things Siemens, read the readme that came with TIA Portal, read the F1-Help for Graph limitations and support to what IEC standard(s), and if you are not satisfied, contact your Siemens distributor and request it get added in a future portal release or update as was already stated.
|
science guy |
|
This contribution was helpful to2 thankful Users |
Follow us on