Industry Online Support
Technical Forum
5/12/2009 5:59 PM | |
Joined: 3/18/2009 Last visit: 5/6/2024 Posts: 306 Rating: (94) |
Hi Nithin, If you are using Step 7, then you don't see the options (channel or module) in CPU H-parameters in hardware configuration. These options are only seen in a PCS7 project. In Step 7, it depends on which library you use for redundant IO configuration. If you have the latest Step 7 version then you can use any of these libraries. For "Channel group" granular -Redundant IO CGP V50" library For "Channel" granular - Redundant IO CGP V40" library For "Module" granular - Redundant IO MGP V30" library. Please remember that only few modules support channel granular redundancy. Check your modules from the list in theSIMATIC Fault-tolerant Systems S7-400H manualbefore deciding on the right library. regards.
|
Last edited by: daga at: 5/12/2009 6:01 PMlink for manual added |
|
Follow us on