2/11/2023 7:24 PM | |
Joined: 2/11/2023 Last visit: 2/13/2023 Posts: 1 Rating: (0) |
regarding unit 6ED1052-1HB00-0BA8: I have version FW V1.08.01 in the device. I have downloaded the file: logo_fw_v1_81_03_up_bm.zip checked the checksum so the file is not corrupted. extracted the ZIP file so the SD card has two files up_bm.bin LOGO_U_P.bin I was expecting that the LOGO should start updating efter power down and power up agian But it does not updating , it starts as normal. I assume that the downloaded file has the FM V1.81.30 and my Logo device should start the pudating process. |
2/11/2023 7:30 PM | |
Joined: 12/18/2014 Last visit: 6/8/2024 Posts: 33165 Rating: (4098)
|
You have a first generation LOGO! 0BA8 and this can't be upgraded. See attached text file. AttachmentVersions of 0BA8.txt (608 Downloads) |
This contribution was helpful to2 thankful Users |
Follow us on