6/9/2023 9:11 AM | |
Joined: 6/6/2023 Last visit: 6/28/2023 Posts: 6 Rating: (0) |
hello guys!! i have a problem to communicate win cc tia portal with Arduino. in fact, i have a shield Arduino and i have watched some tutorial on youtub but all of them does not work !!! sincerely ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/09/2023 10:42:24New subject after splitting |
|
6/9/2023 11:27 AM | |
Joined: 7/19/2022 Last visit: 4/24/2024 Posts: 356 Rating: (60) |
Hello Djamal 44, What communication protocol are you using? A few years ago I managed to communicate an Arduino MEGA with ethernet shield with an S7-1200 through Modbus TCP/IP which I think is the only way through ethernet. There are several examples on youtube although you have probably already seen them. If you are going to read holding registers remember to start at address 40001 |
If this Information really helps, you could use the Rate function |
|
6/9/2023 2:38 PM | |
Joined: 6/6/2023 Last visit: 6/28/2023 Posts: 6 Rating: (0) |
i think that the last line of your answer may be the solution of my problem |
6/22/2023 3:02 PM | |
Joined: 6/6/2023 Last visit: 6/28/2023 Posts: 6 Rating: (0) |
Here in attachment the OPC zip, it's a driver that can permit Arduino and wincc Tia portal to communicate. All we need to do it's to put the IP address in the Arduino scetch and in the connection in win cc Tia portal at the same time! If the IP address is good the will communicate ! Attachmentopc-ua-local-discovery-server-1.04.405.482-20230220.zip (336 Downloads) |
Follow us on