8/15/2023 9:25 PM | |
Joined: 6/11/2019 Last visit: 5/2/2024 Posts: 2188 Rating: (97) |
Hello paylos, As far as I know, you have 64 flags available. Provided they are not used elsewhere ! However, the logo cannot be compared to a real web server and the LWE retains the old data that can arise during a design, although they have been deleted in the editor (see here in the German part of the forum). In addition to the encryption, both of these can lead to the transmission becoming very slow and some packets being lost in the process. Remember that Logo has to work through its program in addition to providing the website. Try the connection not via the markers, but via the variable byts and their bits (VB) greeting Ella_68 (translated with Google) |
8/15/2023 11:35 PM | |
Joined: 12/18/2014 Last visit: 5/2/2024 Posts: 32935 Rating: (4072)
|
Can you upload your LOGO! program and your LWE project as a ZIP file? |
Follow us on