8/21/2023 3:40 AM | |
Joined: 9/27/2022 Last visit: 9/6/2023 Posts: 6 Rating: (0) |
I have another question, After I connect the temperature transmitter with pt100 and with plc (6ED1 052-1MD00-0BA7) I connect it with a power supply 24VDC, it reads 51C, not correct reads why? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/21/2023 10:12:19New subject after splitting |
|
8/21/2023 3:56 AM | |
Joined: 12/18/2014 Last visit: 4/27/2024 Posts: 32894 Rating: (4066)
|
Are you the same user with two nicknames? Jsaidi and JTsaidi? |
8/21/2023 4:11 AM | |
Joined: 9/25/2022 Last visit: 9/18/2023 Posts: 15 Rating: (0) |
temperature range outputs the transmitter (-50 to 150 C) (4-20 mA) check the file in attach, please AttachmentTEMP 2.zip (285 Downloads) |
Follow us on