9/5/2023 12:09 PM | |
Joined: 4/12/2023 Last visit: 9/9/2023 Posts: 1 Rating: (0) |
Hello ! My problem concerns the password to PLC: and the PLC program in my computer. I have not entered a password in the PLC: or in the program in the computer, yet it asks for a password when i try to open. I had a similar program that i could use and open on the computer so i could edit to my liking, now to the strange thing, when i want to open the program again, it requires a password. Why does the program enter a password requirement itself? Which parameter have i clicked on/off? Anybody? this is weird. // Nicklas ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/29/2023 09:33:38New subject after splitting |
|
9/5/2023 2:06 PM | |
Joined: 6/11/2019 Last visit: 4/26/2024 Posts: 2178 Rating: (95) |
Hello nick67sten,
Was the program created with an older LSC version ? And a password was never assigned ? If so, then the bug has definitely struck under LSC 8.3. Sometimes the problem solves itself (perhaps restarting the PC will help). If not, then your only option is to use a Logo 8 to 8.2. This has often been a topic in the German part of the forum (example link). If you don't have an older LSC version and logo, then upload your program. Someone can probably convert it to LSC 8.3 for you. Greetings Ella_68 (translated with Google) |
Follow us on