10/6/2023 1:27 PM | |
Joined: 10/4/2023 Last visit: 10/9/2023 Posts: 8 Rating: (0) |
Do you see any issues with this program?
AttachmentRepeating Loop with 2 limits start stop and safeties.zip (201 Downloads) |
10/6/2023 2:10 PM | |
Joined: 10/4/2023 Last visit: 10/9/2023 Posts: 8 Rating: (0) |
Try this one. If both limit switches are activated at the same time (one sticks and the other is activated) then it stops. If the cylinder does not extend in the set amount of time, activating the limit switch, it stops.
AttachmentRepeating Loop with 2 limits start stop and safeties V2.zip (265 Downloads) |
10/6/2023 3:52 PM | |
Joined: 12/18/2014 Last visit: 4/28/2024 Posts: 32899 Rating: (4067)
|
Try this. You must chance the timer values and the number of loops to your wish. AttachmentRepeating Loop with 2 limits start stop and safeties_V2.zip (206 Downloads) |
10/9/2023 2:35 PM | |
Joined: 10/4/2023 Last visit: 10/9/2023 Posts: 8 Rating: (0) |
Unless I am missing something, the maximum time for step 2 times out regardless if Limit Switch 1 is activated. |
10/9/2023 5:30 PM | |
Joined: 12/18/2014 Last visit: 4/28/2024 Posts: 32899 Rating: (4067)
|
I made a little chance, try this.
AttachmentRepeating Loop with 2 limits start stop and safeties_V3.zip (226 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on