6/10/2024 2:15 PM | |
Joined: 12/18/2014 Last visit: 8/7/2024 Posts: 33498 Rating: (4162)
|
To 1.) Yes. But a download link to V8.3 is no more available, only to V8.4. Can you also use for LOGO! 8.3. Download and installation instructions for LOGO! Soft Comfort Upgrade V8.4To 2.) Yes. To 3.) There is no manual, because the TDE is not programmable. The TDE can only show message texts which you program in LSC. |
This contribution was helpful to1 thankful Users |
Follow us on