9/2/2009 2:51 PM | |
Joined: 4/24/2006 Last visit: 10/14/2024 Posts: 8745 Rating: (1168) |
Hi, See chapter 5.8 Best regards, Wizard |
Last edited by: Wizard at: 9/3/2009 9:15 AMH-H is right, I think I was still sleeping ;-)) |
|
This contribution was helpful to1 thankful Users |
9/3/2009 8:06 AM | |
Joined: 7/2/2008 Last visit: 9/30/2024 Posts: 928 Rating: (308) |
Hello Wizard, MaybeDrozerce has S7-400 module since it has EXTF LED (S7-300 modules have only SF). If it is S7-400 module then chapter 5.17 should be read in SIMATIC S7-400 S7-400 Automation System Module Data. I also do recommend to check the hardware online. I believe it should be either indicated in diagnostic buffer or the module itself should be marked in red with a diagnostic message in hardware configuration online window. Best regards. H-H |
This contribution was helpful to1 thankful Users |
9/7/2009 9:59 AM | |
Joined: 4/24/2006 Last visit: 10/14/2024 Posts: 8745 Rating: (1168) |
Hi drozerce, Great, you solved your problem Best regards, Wizard |
Follow us on