5/18/2010 7:09 AM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477) |
Well I have seen this too...
Its not necessary that you can always use control panel for Masterdrive. I have seen in some compact drives that this option doesnt come. I also noticed one more thing for these type of drives. In trace function, the option for binector trigger is disabled means we can not give binector as a trigger. See attached file. This occurs in the drives in which we can not use control panel Regards, Devesh AttachmentTrace.pdf (227 Downloads) |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
Follow us on