Industry Online Support
Technical Forum
10/23/2010 5:51 PM | |
Posts: 3609 Rating: (29) |
|
10/24/2010 9:11 AM | |
Posts: 2964 Rating: (481) |
Hi.... > GUDs are the variables which can be used globally and can be called by their names. >The data type can be anything integer, charecter, string, real or array.>These are divided in two categories, NCK as global and CHAN as channel specific.>Total 9 GUD areas can be definedSGUD ® 1 ; Reserved for SiemensMGUD ® 2 ; Reserved for OEMsUGUD ® 3 ; Reserved for USERGUD4-9 ® 4-9 ; Available for all I am attaching you the details of the same for the reference...Check it out... Regards, Ekalavya AttachmentGUD.pdf (558 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on