5/6/2011 8:18 AM | |
Joined: 10/7/2005 Last visit: 11/19/2024 Posts: 3027 Rating: (1057)
|
Hello lisalxy Yes it does. It ultimately means that you will find the Integer number "141" in DL 53. After execution of "LW =A-DB" Accu1-L will contain a value of 141 in the Low byte and anotehr 'bitpattern" value that representsthe "DB" part of the parameter declaration in the high byte (which is typically of no use and in this case the programmer was definitely only interested in getting the DB number) I hope this helps |
Cheers |
|
This contribution was helpful to2 thankful Users |
5/6/2011 8:43 AM | |
Posts: 24 Rating: (0) |
Thanks fritz! That clears my problem! |
This contribution was helpful to1 thankful Users |
Follow us on