Industry Online Support
Technical Forum
8/29/2011 5:53 AM | |
Joined: 7/17/2010 Last visit: 2/17/2024 Posts: 184 Rating: (0) |
Sorry I will attach. What I do is the following. Operator will entar with a value in m / min and will charge via HMI, there will have a proportional output 0-10V, there comes the bid effort if the engine has a lot of effort will have a pot to take this and twist into anger with a signal of-5V there have to further accelerate the motor up and stabilize voltage comes back close to zero, if the engine got very little effort will have a voltage up to +5 V i have to slow the engine to get the signal from the potentiometer again close to zero and return the speed entered by the operator: example 30m/min inserts the TD-200 if the voltage goes into the pot is getting negative or-5v have to rev the engine to compensate if the voltage goes into the pot that is getting positive 5v have to decelerate the motor to compensate AttachmentBALANCIM.pdf (120 Downloads) |
Follow us on