Industry Online Support
Technical Forum
10/13/2011 7:49 AM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating: (1181) |
Hello, Attach here a screenshots of ALM. Meanwhile use Support Request option... Best regards, Hristo MIhalev |
10/13/2011 10:47 AM | |
Posts: 270 Rating: (53) |
Hi Henio, I'm just wondering, isn't it possible that you have the licences to the mentioned programs accessed online (through a server, if I understand http://support.automation.siemens.com/WW/view/en/25619730right, it's possible) and you somehow lost connection to it (i. e. joined some other wifi, because the access to the other is limited in order to prevent access from anywhere) or some sort of cause like this? It's a long shot in the dark, but maybe? :) |
10/13/2011 11:40 AM | |
Joined: 4/24/2006 Last visit: 8/15/2024 Posts: 8715 Rating: (1166) |
Dear Henio, Please have a look at the following link: Why does a message appear in STEP 7 stating that there is not a license key present even though the relevant license key is installed? Try point 2. Or else try the following: Presumably there is a write protection on a MachineKey folder which blocks the Automation License |
10/13/2011 7:11 PM | |
Posts: 53 Rating: (2) |
Hi, i tried Why does a message appear in STEP 7 stating that there is not a license key present even though the relevant license key is installed? point 2 yestrday without any result. But the second advise IS WORKING !!! Thank You very much man :) (i were preparing to reinstall step7/windows :( ). Best regards, Henio. |
This contribution was helpful to1 thankful Users |
Follow us on