4/9/2013 4:58 AM | |
Posts: 39 Rating: (0) |
Thank you Eastern for your kind reply. I don't think so there is any problem with the PLC memory slot, B'coz when I insert the other SRAM card, it detects and I find no problem in downloading the program. But when I insert the Flash card EXTF LED is ON and STOP LED blinks at around 1 hz. Could there be any possibility that my flash cards have problem? and am I following the proper procedure to download the program to Flash card? Thanks in advance Regards, Ujwal Sadare
|
4/9/2013 5:00 AM | |
Posts: 39 Rating: (0) |
and when I go online I do not detect any Memory card and hence it does not download. I have tried with another Flash card with same MLFB no, perhaps same result
|
4/9/2013 7:46 AM | |
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
Hello ujwalsadare, Try to Checked the Slot of the Memeory card is any Pin inside is not get bend, this might be a problem, |
Ammy |
|
4/9/2013 2:44 PM | |
Posts: 557 Rating: (64) |
Hello, According to Ammy this could also be a problem some time we insert card with wrong direction therefore it cause damage something. Certainly your menory card is not detected by PLC. As you said other cards are working with CPU that mean MC card has some problem. |
4/10/2013 2:14 AM | |
Posts: 39 Rating: (0) |
Hello Ammy, Thank you for sparing your time. I have checked the memory card and there are no hardware damages as such. Pin seems to be fine. Not sure what else could go wrong Regards, Ujwal Sadare |
Follow us on