1/12/2014 10:50 AM | |
Posts: 8946 Rating: (999) |
Try a masterreset, remove Memory Card if exist. Perhaps, CPU is damaged. |
1/13/2014 11:44 AM | |
Posts: 34 Rating: (0) |
Dear Barain Check Hardware Configuration if it is any thing wrong this will make this error Regards |
1/22/2014 1:32 PM | |
Joined: 8/20/2011 Last visit: 9/20/2024 Posts: 22 Rating: (0) |
HiBahrain123 Check the Backplane pin between CPU and Rack Try to take Master reset with HOTKEY for 5 secs. Thanks DINESH
|
2/11/2014 1:04 AM | |
Posts: 1 Rating: (0) |
Did you find a fix? |
2/11/2014 4:38 AM | |
Joined: 1/28/2009 Last visit: 10/26/2024 Posts: 6852 Rating: (1365)
|
Hello, There are some possibilities and remedies but the easiest way to select would be sending the faulty CPU to your local repair shop.In addition to all discussed topics here,I add a quoted post from HERE:
I hope you are lucky enough and one of the discussed possibiities solve your case.I guess, we reach to the point to receive a Draft of an FAQ for similar fequently occured errors and again "Marking another thread as FAQ" sounds less convincing. Best regards, Hamid Hosseini |
This contribution was helpful to2 thankful Users |
Follow us on