11/5/2007 12:07 PM | |
Posts: 4 Rating: (0) |
I'm trying to create a specialized programwherein an on/off delay relay holds an output open when an input is switched off and back on. Attached is the program, but the Q2 and Q3 outputs are reset whenever the corresponding inputs are switched off and on, and I need them to stay on during a break of input lesser than the off delay. Any ideas? I've been fighting this otherwise simple switching program for days. Note: File is not a ZIP, I just changed the extension from .lsc AttachmentShutoff with delay.zip (645 Downloads) |
11/6/2007 3:12 AM | |
Posts: 191 Rating: (58) |
Please try this.. if it doesnt work post again.. ROSA AttachmentShutoff with delay2.zip (551 Downloads) |
11/6/2007 10:35 PM | |
Joined: 1/5/2007 Last visit: 4/7/2023 Posts: 1690 Rating: (580) |
Hello MEP1, look at the attachment for my solution of your question. I hope that is what you wont! Best regards Betel AttachmentShutoff with delay 3.zip (639 Downloads) |
==> Meine TAG-Listen: "deut." |
|
Follow us on