5/21/2015 7:56 PM | |
Joined: 1/25/2006 Last visit: 7/27/2024 Posts: 257 Rating: (60) |
Unfortunately, on those eeproms (two), I have no that number!! Those are used eeprom which I want to reprogram. |
5/30/2015 11:14 AM | |
Joined: 11/21/2007 Last visit: 7/7/2024 Posts: 2325 Rating: (307)
|
Hello The Prog No of the EPROM can be seen in the STEP5 help diring EPROM selection. There is a complete list in the Directory : S5_SYS in the file S5EPROMS.PTE ( I have attached this as a TXT file here ) As per the list The Prog No of 6ES5 375-0LC31 is 211 Hope this helps Cheers Navnag AttachmentS5EPROMS.TXT (378 Downloads) |
There is no such thing as the last bug in a program |
|
Follow us on