10/19/2016 12:57 PM | |
Joined: 4/28/2015 Last visit: 5/15/2024 Posts: 3345 Rating: (377)
|
Hi, yes, the recipes from openembedded can be used. How to include them you can find in this post. Add the layers including your recipes needed via gitclone. Then add the cloned folders to the bblayers.conf. This two steps are described in the linked Readme for the Example Image layer. To include the packages to the image to build open /recipes-core/images/core-image-minimal.bb on your building systems and add: IMAGE_INSTALL_append = "name_of_package" I hope this information is helpful and you can follow me ;) Best regards |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on