11/3/2016 5:30 AM | |
Joined: 11/23/2015 Last visit: 5/22/2024 Posts: 14 Rating:
|
Hi Every body I had a problem with DB in my program, this is error "There are no parameter and local variable names available because there is a time-stamp conflict between block interface of the blocks and the description of parameter and variable name". So when i download change the FC (FC in FC), the Sub FC canot run (the Input value of FC are the DB values). Then we must download the original FC again to CPU and they are running normal. I dont understand why it happen like that. Thanks! AttachmentDB ERROR.pdf (249 Downloads) |
11/3/2016 8:40 AM | |
Joined: 11/23/2015 Last visit: 5/22/2024 Posts: 14 Rating:
|
Hi STE39, I compared it, it is different Time-stamp. I think that is not a problem. |
Follow us on