4/11/2014 7:11 PM | |
Posts: 7 Rating: (0) |
Hi, Its showing Parameter assignment error in Diagnostic Buffer. please find the ATTACHMENT
AttachmentUntitled.zip (256 Downloads) |
4/12/2014 4:45 PM | |
Posts: 7 Rating: (0) |
Hi, Please find the diagnose
AttachmentNew folder.zip (258 Downloads) |
4/12/2014 6:22 PM | |
Posts: 7 Rating: (0) |
Hi, Thanks for your suggestion. I tried with that sync module , but no change. |
4/14/2014 5:35 AM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365)
|
Hello, I have tested the situation with different order number for Sync.Modules and my CPUs were in RUN status without problem(attached file).I tried several scenarios to re-create same messages as logged in your case, but not possible. Finally,I suggest uploading buffer of both CPUs here with correct date and time because logs of partner will help us the most to understand the whole situation.You can try sending your log and project to HERE for possible help. Best regards, |
5/23/2014 7:53 AM | |
Posts: 73 Rating: (6) |
Hi, It would also make sense to download Error OBs [OB71, OB72, OB80-87, OB121, OB122] into the CPU to prevent CPU from going into STOP mode. Regards, Krrish !! |
1/25/2018 1:00 AM | |
Posts: 1 Rating: (0) |
Hi, I have had the same issue as above but when i add the suggested OBs they are deleted during a compile. Can you please advise on how to fix this?? Thanks |
Follow us on