3/9/2018 7:02 AM | |
Posts: 69 Rating: (4) |
I can't communicate drive with starter using profibus. Evertime I try, it says no devices found! How can I do that? Also, what all parameters should be entered while quick commissioning? I am getting F60056 fault. I have given all the motor data from name plate and p50083 set as 1. What all shall I do for quick commissioning without fault? My drive is not connected to motor. ------------------------------------------------------------------------------------------ |
Last edited by: Masru at: 3/9/2018 8:06:52 AMLast edited by: The Helping Hand at: 3/9/2018 9:48:30 AMNew subject after splitting |
|
3/9/2018 10:43 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873) |
Yes. Unless & until motor data & controller parameters are set/calculated, how drive will work? |
3/9/2018 10:48 AM | |
Posts: 69 Rating: (4) |
How can we calculate the % value to be given in p50076? Also what values shall be given at p50078? Are they the rating values given outside the drive cover? |
Follow us on