5/3/2018 2:48 PM | |
Posts: 1 Rating:
|
Can anybody tell me if we can power the Sinamics V20 Inverter rated at 400V with only 2-leg, line-to-line 400V? Mains Terminals are labelled as: L1, L2/N, L3. Their 230V units have mains labeled as L1, L2/N. Both of the 230V & 400V units output to motor is 3-phase. ------------------------------------------------------------------------------------------ |
Last edited by: NoliM at: 5/3/2018 2:51:31 PMLast edited by: NoliM at: 5/3/2018 2:51:44 PMLast edited by: Jen_Moderator at: 5/4/2018 7:40:22 AMNew subject after splitting |
|
Follow us on