Industry Online Support
Technical Forum
10/23/2018 5:02 PM | |
Posts: 1 Rating:
|
We have drive 6SE7021-3TB61-Z and switched out the CUVC card 6SE7090-0XX84-0AB00 and when commanded to run get a F008 DC bus link fault. Installed the CUVC card in another drive and problem follows the card. I see that the firmware chips are different, original 0A0B314, new card 0A0B323. Could these chip differences cause this? Is there a process to recognize an updated firmware chip? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/24/2018 9:28:39 AMNew subject after splitting |
|
11/16/2018 7:56 AM | |
Joined: 1/16/2015 Last visit: 6/14/2024 Posts: 46 Rating:
|
In which situations is the F008 coming? Did you adjust the P70 to match the power section? |
Follow us on