4/6/2019 7:39 AM | |
Joined: 3/6/2017 Last visit: 2/5/2024 Posts: 8 Rating: (0) |
Dear Experts, I want to test fault signal lamp connected at DO2 using any connection macro, cn002 for example, as in the attachment. If any external fault occurs, disconnected any phase from the inverter to the motor for example, the fault signal lamp DO2 shall be illuminated. If the fault is cleared and/or fault is acknowledged via input DI3 the lamp goes off. Can anybody assist me in doing the test? How the configuration shall be done? AttachmentV20_op_instr_0618_en-US 69.pdf (86 Downloads) |
Follow us on