5/21/2019 10:30 PM | |
Joined: 9/27/2006 Last visit: 5/15/2024 Posts: 12257 Rating: (2668) |
Hello kakoskilo; Have a look at he the following discussion, joined by our most knowledgeable TI 505 experts, Sam the Eagle and Bill West: Where can i get the TISOFT/SOFTSHOP software? TISOFT is the original, DOS-based, programming software for the TI 505 CPUs. You can download the file from the discussion above. Fast-Soft now sells a Windows-based product named PLC WorkShop Suite for Siemens 505. The programming port on the CPU uses a standard RS-232 cable, as seen from the attachment below. The port must be configured by the use of dipswitches on the CPU board. This image is extracted from this manual, which you will need: 505 System manual https://support.industry.siemens.com/cs/us/en/view/17514935 This manual might also be very useful to program a TI 505: 505 Programming Reference https://support.industry.siemens.com/cs/us/en/view/17514825 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 05/21/2019 22:31:56 |
|
This contribution was helpful to1 thankful Users |
Follow us on