6/29/2019 10:58 PM | |
Posts: 2 Rating:
|
Dear Experts, I'm working in automation project, I've bought next parts: -> SIMOTICS S-1FL6 1FL6034-2AF21-0AA - 0.4kW - 2.6A - NN=3000rpm - M0=1.27Nm - ENCODER TTL 2500 incr/rev -> SINAMICS V90 6SL3210-5FB10-4UF1 - 3AC200-230V - 2.6A - 0.4kW - IP20 I need to do a Speed Control in a machine, I've connected the v90 and the servomotor, I'm programming in V-ASSISTANT, I can move the motor trought the software, But I can't move the motor trought IO terminals block, I can read the voltage in analog input, but I don't know what is the digital input that let me start the motor, I've combined some terminals to start the motor, but no success. I've attached some pictures about the configuration I've done, I'l be gratefull if you can help me, Thanks a lot, Regards,
Attachmentdoc1.pdf (106 Downloads) |
6/30/2019 5:18 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Please refer SINAMICS V90 Pulse train, USS/Modbus, SIMOTICS S-1FL6 Operating Instructions manual, page 258, speed control with external analog speed set point, will help you to set appropriate parameters. HTH |
Last edited by: Jen_Moderator at: 07/01/2019 12:28:24Optimized link. |
|
Follow us on