9/6/2019 2:04 PM | |
Joined: 10/11/2006 Last visit: 7/12/2024 Posts: 5874 Rating:
|
Dear _oleksandr_, both encoders can be found in the Catalog D81.1 (https://support.industry.siemens.com/cs/document/109749197). The LL encoder is "G04", the HOG encoder as "G06". Both are heavy duty encoders., G04 from LeineLinde G06 from Baumer. Directly from the Catalog: G04 offerst IP65, G06 IP66. G06 offers a higher temperatur range. Depends on the application.and the conditions they are used in. |
With best regards, |
|
Follow us on