4/14/2020 1:43 PM | |
Joined: 9/30/2016 Last visit: 11/11/2024 Posts: 914 Rating: (6) |
Please also see the attached screenshots. We have a turntable that is turned by two DC drives in master-slave configuration (I have been told that the masters current is used as a setpoint for the slave so that the 2 drives should end up sharing the load by using the same effect. In the current running mode we have chosen to only run on one drive (luckily they are powerful enough to run in single mode) since the slave drive for some reason stops by itself and generates alarms after running a few hours as slave. But drives have done this while running in slave mode. When it is running with a single drive it does not stop. Once they have stopped the can be reset right away and restarted - but we don't want to have to do this all the time so we want to find out why it is stopping and correct it. AttachmentGH11A.zip (299 Downloads) |
4/14/2020 1:48 PM | |
Joined: 5/12/2006 Last visit: 11/11/2024 Posts: 22445 Rating: (3029)
|
hi, and generates alarms after running a few hours which alarms? Christoph |
Follow us on