6/23/2020 12:04 PM | |
Posts: 3 Rating: (0) |
Hello, I'm about to make my graduation project about automating a "sheath cutting machine", which i'll use a PLC to command it but i'm lost choosing the right one, i thought about the S7-1200 but need extensions i think. 2 D.O 1 A.O 5 D.I 4 A.I Thanks helping me picking the right one. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/23/2020 14:12:14New subject after splitting |
|
6/23/2020 2:13 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject Choosing a PLC is published within the conference SIMATIC S7-1200. Best regards,Jen_Moderator |
Follow us on