6/15/2020 7:29 PM | |
Joined: 12/31/2018 Last visit: 3/10/2024 Posts: 96 Rating: (3) |
Hello Everyone, I have tested the Flex Client with the same network switch, but it requires to be accessed by the person who is on the other network switch. scenario is, We have BMS network switch which is connected to client network at Network Switch-A, now am able to access Flex client (or ClickOnce) from this Network switch. but I try from another network switch-B, am only able to reach the Log in page-it shows No connection to management Station. Network switch-A has IP range 172.19.20.X and network switch - B has another IP range and different Subnet mask. I am able to ping the server from anywhere in the network, but could not log in to Flex Client, what settings I have to do to communicate over different IP range or Different Subnet mask? or issue cab be different? (Client IT team has told there is no blocking at network level) Regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/23/2020 14:15:47New subject after splitting |
|
6/23/2020 11:04 AM | |
Joined: 12/31/2018 Last visit: 3/10/2024 Posts: 96 Rating: (3) |
Hi I have attached the Error file creating while downloading the ClickOnce. Can anyone please help me to find a solution. regards AttachmentApp Download Log.txt (319 Downloads) |
Follow us on